MLFB_HomeFindZeroAngle
Function Block - Homing to zero angle reference.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
ibExecute |
BOOL |
FALSE, TRUE |
N/A |
No default |
Start homing, edge-triggered. |
iAxisID |
DINT |
|
|
|
ID of the axis block of the Pipe Network. |
iPosition |
LREAL |
|
|
|
Reference position. |
iDirectionType |
DINT |
|
|
|
|
iVelocity |
LREAL |
|
|
|
Reference speed. |
iAcceleration |
LREAL |
|
|
|
Reference acceleration. |
iDeceleration |
LREAL |
|
|
|
Reference deceleration. |
iTimeout |
TIME |
|
|
|
Time monitoring (T#0ms: off). |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
obDone |
BOOL |
FALSE, TRUE |
N/A |
Done bit. |
||||||||||||
obActive |
BOOL |
FALSE, TRUE |
N/A |
Active bit. |
||||||||||||
obError |
BOOL |
FALSE, TRUE |
N/A |
Error bit. |
||||||||||||
oErrorID |
DINT |
|
N/A |
Error identifier:
|
Remarks
-
- This function block is only applicable to motors with Resolver or SFD feedback.
|
|
Figure 1: Mode to find the zero angle reference of the motor.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Call homing function on Axis1 with preset velocity, accel, and decel values
//Start in negative direction and go to zero angle or time out
//after reaching zero angle set axis position to zero
Inst_MLFB_HomeFindZeroAngle( StartHomeRoutine,
PipeNetwork.AXIS1,
0,
1,
100,
1000,
1000,
T#30s );
HomeDone := Inst_MLFB_HomeFindZeroAngle.obDone;
See Also