Motion / Pipe Network

The KAS-IDE function library contains Motion Library (ML) function blocks (FBs) used to integrate motion from a Pipe Network in a PLC program.

These are the ML function blocks:

Function

Description

Block

Manage the blocks: Create / activate.

See Block for more information.

Motion

Prepare the physical motion part: init, reset, start, stop.

See click here... for more information.

Pipe Block

Manage each specific Pipe Block: Read / write parameters.

The function blocks are:

Pipe Network

Manage the Pipe Network: Create / activate.

See click here... for more information.


  • Pipe Network code is generated automatically by the compiler.
    Do not try to modify it.

Concept Link IconSee Also