Define Method Parameters


  • Verify the Create a Method procedure is completed before defining a method.

Each method has its own interface definition independent of the parent UDFB implementation.

A method interface can contain:

  • Input parameters.
  • Output parameters.
  • Local variables.

Examples

Input Parameters

Name

Type

Description

Position

LREAL

Target position

Velocity

LREAL

Requested velocity

Output Parameters

Name

Type

Description

IsValid

BOOL

Validation result

ErrorCode

DINT

Validation error

Local Variables

Name

Type

Description

MaxVelocity

LREAL

Internal limit

TempError

DINT

Working variable


    • Local variables declared within the method are only accessible from that method.

See Also