TxPDO - AKD Drive CANopen Objects
This table identifies:
- The CANopen objects required by the motion engine and function blocks.
- Whether the objects are available in the default PDO
PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices.. - Their corresponding drive parameter.
-
-
Review the table to verify the objects needed by the features the application uses are included in the PDO selection.
|
Index - subindex |
Object Name |
Required |
Associated ML FB |
Associated MC FB |
Associated Drive Parameter |
|---|---|---|---|---|---|
|
0x6041 - 0 |
|
Yes |
N/A |
N/A |
N/A |
|
0x6063 - 0 |
Position actual value |
No |
|
|
|
|
Position actual value 2 |
No |
MLAxisRead2ndFB
|
|
(If DRV.CMDSOURCE = 1) |
|
|
0x606C - 0 |
Velocity actual value |
No |
|
|
|
|
0x6077 - 0 |
No |
|
|
|
|
|
0x20A5 - 0 |
No |
|
CAPx.STATE |
||
|
0x20A6 - 0 |
Latch position |
No |
|
|
|
|
0x60FD - 0 |
Digital inputs Used by Onboard I/O mappings |
No |
N/A |
N/A |
|
|
0x3470-4 |
AIN.VALUE Used by Onboard I/O mappings |
No |
N/A |
N/A |
AIN.VALUE |
|
0x60F4 |
Following error |
No |
|
|
|