FAQs
Basic
The Autorun feature may be deactivated.
- Open an Explorer window to see the autorun.exe file.
- Use the Run command in the contextual menu to manually start the installer.
That depends on the version of KAS Kollmorgen Automation Suite.
You may have one version of KAS-IDE Kollmorgen Automation Suite - Integrated Development Environment v3.00 and earlier installed along with any number of later versions.
KAS version | Only 1 version |
|
---|---|---|
< v3.00 | ||
v3.01 and later |
Yes, as long as one of the versions is v3.02 or later.
With the release of v3.02 multiple instances of the KAS-IDE Integrated Development Environment - An type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger. are permitted.
That includes running one older (<v3.02) instance and any number of newer instances. This includes multiple instances of the same version. The only limitation is available RAM.
The default version of the KAS-IDE is the one most recently installed.
This can be changed to a preferred version by changing an Environment Environment objects are global objects that exist before the execution of the script. Typically, they are global objects of Astrolab that can be accessed from the script. Variable.
From the list of System variables, edit KAS_INSTALL_DIR. Enter the path Set of continuous positions and orientation information in multi-dimensional space. Geometrical description of a space curve that the TCP of an axesgroup moves along. to your preferred version.
Yes, the KAS-IDE supports copying and pasting between simultaneously running instances.
- This is supported in both the same version and different version numbers.
- This includes drag and drop for supported objects (e.g., FBD Function block diagram - Describes a function between input variables and output variables. A function is described as a set of elementary blocks. blocks).
The KAS-IDE attempts to recreate what you have copied, but there are some limitations.
Example: It may not automatically associate variables with a function A function calculates a result according to the current value of its inputs.
A function has no internal data and is not linked to declared instances..
If you copy and paste only a function block A function block groups an algorithm and a set of private data.
It has inputs and outputs. from an FFLD program, the assigned variables is not copied and pasted.
If you select the entire network, the KAS-IDE automatically creates the variables for you.
Copying a block | Copying an entire network recreates assigned variables in the Dictionary |
-
- Closing the KAS-IDE automatically clears the Clipboard.
Anything that was copied is cleared from memory.
This means you can not copy something, close the KAS-IDE, and then paste.
A side effect with some remaining files that were not deleted properly can interfere with your new project. To fix this issue:
- Close your current project without saving.
- Open Windows Explorer and go to C:\Documents and Settings\(user)\Local Settings\Application Data\Kollmorgen\KAS\Project, where “(user)” is the Windows' username you are currently logged in with.
- Delete all the remaining files and folders.
- You can now create your new project.
Everything in our manuals may be found in the online help.
If you need a printable document or want stand-alone manuals, the documentation is available as PDFs on KDN.
With the AutoSave function, project files are saved for recovery.
More than one file may exist due to multiple versions of the KAS-IDE being installed or used.
- When you restart the KAS-IDE you are prompted to recover a found file.
- When there is more than one file, the recovery process starts with the latest date from the newest KAS-IDE version.
- Assuming you choose to recover the file it is opened and you may resume work but the older recovery files still exist.
The next time you launch the KAS-IDE, you are prompted to recover the next oldest file. Choosing to not recover the file will delete it, and you are prompted to open the next oldest file until none are left.
Computer / Controller
This number is mainly dependent upon the application and your PC Personal Computer's computing power.
An average number would be 20 axes/ms.
This procedure allows you to determine if your controller is overloaded due to the PLC Programmable Logic Controller - A digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events. program or motion system load.
You can use the Softscope and the Trace Times button to display these CPU loads:
- Cycle Jitter The difference between the configured cycle time and the actual meausured cycle time. Unit is in microseconds. (microseconds)
- Motion execution time (microseconds)
- PLC execution time (microseconds)
- Real Time Margin (microseconds)
To view the load:
- Open the Softscope.
- Plug four probes See Softscope - Probe item. to any kind of data.
See Mapping a Variable to the Oscilloscope. - In the Control Panel, click the TraceTimes button.
If you are unable to log into the controller's webpage using a valid user ID and password, the controller's file system may be corrupt.
To recover the system you will need to use the push buttons on the controller (see Boot from Recovery Image (B2 Button)) to recover the system.
Graphics need to be made portable with a project, otherwise the KAS-IDE attempts to point to the original location of the graphic files.
To make graphics portable, copy them to
C:\Users\[user folder]\AppData\Local\Kollmorgen\Project\Controller\PLC.
After this the graphics are a part of the .KAS file.
On the PCMM2G, the time is incorrect if all these conditions are TRUE:
- The controller looses power.
- Network Time Protocol (NTP) is disabled Removal of the ENABLE signal. Disables power stage..
- There is no battery backup.
EtherCAT
An E33 occurs when the EtherCAT network fails to start when first loading a KAS project.
This typically occurs when the devices on the EtherCAT network do not exactly match the ENI file inside the KAS project.
- This can mean that devices were added, removed, or put in a different order.
- If this happens with a machine The complete assembly of all connected parts or devices, of which at least one is movable. in the field that was working, it means that one or more devices are no longer being seen on the EtherCAT network because they are not powering on or an Ethernet Ethernet is a large, diverse family of frame-based computer networking technologies that operate at many speeds for local area networks (LANs). cable came unplugged or broke.
Error Correction:
- Check the EtherCAT network wiring and devices state.
- Re-start the application.
- If you have the KAS-IDE software, you can scan the EtherCAT network to see if all the devices are found and in the correct order.
See ESI and ENI Files.
No. As with every real-time Industrial Ethernet system, one device (the master) has to be in charge of the network management and organize the Medium Access Control. With EtherCAT, Slave-to-Slave communication is supported either with:
- Topology dependent within one communication cycle ("upstream" device talks to "downstream" device).
- Topology independent within two cycles.
Since EtherCAT is so much faster than competing systems, slave-to-slave communication, using two cycles is faster.
The maximum number of node addresses is 65,535.
Typically, the number of the nodes on the network is limited by the maximum EtherCAT frame In networking dialect, a message is called a frame. size, which is 1500 bytes.
See the Frame Size in the EtherCAT Master Settings tab for more information.
-
Depending on the number of AKD drives In electrical engineering, a drive is an electronic device to provide power to a motor or servo. Control device for regulating the speed, torque and position of a motor. A unit controlling a motor using the current and timing in its coils. physically present in the EtherCAT network, the KAS-IDE might slow down when getting data.
The KAS Runtime In computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). In KAS, runtime refers to the virtual machine that manage the program written in a computer language while it is running. is not concerned with this limitation.
If you need to rely on SDO communication to set the parameter of an EtherCAT device, you can do this with the ECATWriteSdo FB
See Fieldbus - EtherCAT.
Being asynchronous and based on the EtherCAT mailbox, the SDO communication is not deterministic.
- The EtherCAT master uses a polling mode to ensure the SDO command is completed.
- In operational mode, this polling is performed every 50 cycles 1.
- As a consequence, you can expect the acknowledgment of your SDO command usually before less than 100ms.
- A good practice is to set the update rate for SDO communication in your PLC application each 25 cycles.
See also see "EtherCAT Motion Bus Concepts" on page 1 for more information.
The AKD2G has a limit on the number of PDO Process Data Opjects - A type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. objects which can be mapped, depending on the sample rate.
Sample Rate | Cycle Time | Max. PDOs |
---|---|---|
4kHz | 250μs | 14 Rx, 14 Tx |
2kHz | >500μs | 30 RX, 30 Tx |
This limitation can be hit during compilation with this error:
EtherCAT: ERROR: In AKD2G_1, the total number of entries for all selected Tx PDOs is greater than the max allowed at a cycle time of 250 μs: 17 > 14
There are three possible solutions.
- Increase the Cycle Time – see EtherCAT Master Settings tab
- Deselect unused PDOs – see PDO Selection/Mapping tab
- Delete unused objects – see Delete a CoE Object
When the application runs on the KAS Simulator, the PLC execution rate is approximately 10ms.
KAS Simulator cannot execute the PLC programs faster because Windows is not able to handle timing less than 10ms.
Performance
It is generally recommended to use USB Universal Serial Bus - A serial bus standard to interface devices. 3.0 (USB - Wikipedia) or higher standard on the PCMM2G to have a better performance.
The normal recovery image boot up is around 30 to 40 seconds.
- If the controller 7-segment display is for a longer period Motor systems having a reciprocating or oscillating motor that operates synchronously with the periodicity of the source which supplies the electrical energy. The period of execution of a pipe is the time spent between two successive computations of set values for the same pipe. The period of execution of a pipe is specified by the PERIOD parameter of the input pipe block. of time (more than two minutes), this delay could be because the recovery image is being flashed to an incompatible USB flash drive.
- This delay may not prevent the user from following the recovery procedure.
- See Boot from Recovery Image (B2 Button) for more information.
Contact Kollmorgen Technical Support if the issue is still not resolved using a USB 3.0 or higher.
Due to excessive ASCII American Standard Code for Information Interchange - ASCII provides a one-to-one mapping between alphanumeric characters and a digital one-byte word. SDO commands or very slow Ethernet communication, the WorkBench tree may not fully populate or navigation may be unresponsive.
To recover from this situation:
- Click the Refresh GUI command that re-loads the data from the drive and redraws the display. Tree button in KAS-IDEWorkBench view.
- Disconnect and Reconnect the KAS-IDE to restart KAS-IDE-WorkBench communication.
The status bar may display a warning if communication between the KAS-IDE, controller, and drive is too slow.
To begin troubleshooting, configure the Local log for WARNING level (or lower) and check for "communication too slow" messages.
The IDE-WorkBench navigation and views may become very slow or completely unresponsive if the average response time for drive communication is too long.
Communication delays between the KAS-IDE and Controller can be caused by degraded Ethernet bandwidth In computer networking, bandwidth refers to a data rate measured in bits per second (e.g., network throughput). The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz. In a servos system, the frequency at which the small signal response begins to drop off. Stage performance is enhanced by increasing the servo bandwidth. Structural resonances typically limit the achievable bandwidth. or high latencies.
You can use the Windows Resource Monitor (resmon.exe) and select kas_ide.exe to monitor and diagnose high latency and/or poor bandwidth.
Communication delays between the Controller and Drive can occur while an application is running on the controller.
Degraded drive communication can be caused by excessive ASCII SDO commands from the application code.
- Check your application code for calls to DriveParamRead/Write(...), DriveParamStrRead(...), or ECATRead/WriteSdo(...), and minimize the frequency of these calls.
- Use Online Configuration Mode with KAS-IDEWorkBench to avoid ASCII SDO channel competition between your application and KAS-IDEWorkBench
There are times when trying to connect to multiple drives simultaneously with WorkBench is problematic, particularly on slower networks.
Resolution
- Close all of the open windows in the IDE workspace, leaving only one WorkBench window open.
- Connect the KAS-IDE and run the project or use Online Configuration mode.
These actions reduce the network and KAS-IDE loads. This allows the embedded WorkBench to establish communication and access the views.
To access multiple drives at the same time:
- Open one WorkBench window
- Wait for communication and initialization to complete successfully
- Open each additional WorkBench window one at a time.
Allow enough time for each to successfully complete initialization.
Programming
When you want to check the maximum time execution for an SFC Sequential function chart - It can be used to program processes that can be split into steps. The main components of SFC are: - Steps with associated actions. - Transitions with associated logic conditions. - Directed links between steps and transitions. step, you have to program this action based on the SFC alarm capability.
To show this status:
- In the Dictionary, declare a Boolean PLC variable linked to the related SFC program.
- Add the instruction in the Actions tab related to the SFC step, with first parameter set to A (for Alarm).
The syntax is explained in Actions in an SFC Step.
More details on the timeout on an SFC step are in Timeout on an SFC Step.
If you open a project containing a link on a library which is no longer available, a warning is displayed. To fix this issue, refer to (➜ # 1, What happens when a library no longer exists?)
The Fast Input The inputs are taken into account at each cycle depending on the system periodicity (i.e., each millisecond). Under certain circumstances, this can be insufficient when more accuracy is needed or if a quick response is required from the system. To fill the gap, a drive may have some Fast Input connections (generally one or two). When an event happens that triggers a Fast Input (e.g., when a sensor sends a rising edge), the detection of a signal occurs faster. This can be 1000 times more accurate than the system periodicity. The timestamp associated with this input can be provided to the IPC to take corrective action. allows an application to get information about the occurrence of an external event at a higher resolution The resolution is the smallest possible movement that can be achieved by a system. It can be defined at the electronics, encoder and mechanics level. The distance a stage can be commanded to move in a single step. For servo systems, the basic increment produced by its optical encoder, or any other feedback device. than the cycle time.
For more details, see Fast Inputs with Pipe Network Motion.
There are two kinds of feedback:
Primary Feedback
- With a S300 Servostar 300 drive drive you can use a resolver for primary feedback.
- If a secondary feedback is required with your S300 drive, you can use a BiSS Bi-directional Serial Synchronous interface - An open-source communication protocol for feedback devices.
With BiSS, all of the computation for interpolation in regard to position occurs on the ASIC directly in the encoder. feedback device A process where some proportion of the output signal of a system is passed (fed back) to the input.
In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position.
Some systems use a feedback device connected to the motor shaft or part of the driven mechanism to control the direction, acceleration and speed of the motor..
- If you use the same setup with an S300 drive, the S300's EXTPOS parameter has to be set to -11.
IMPORTANT: do not omit the negative sign! - To access secondary feedback, use a SAMPLER Pipe Network block.
- If you use the same setup with an S300 drive, the S300's EXTPOS parameter has to be set to -11.
- Use the MLSmpConPNAxis, MLSmpConPLCAxis, or MLSmpConECAT functions to configure the block.
Current drives that support torque The tendency of a force to rotate an object about an axis. A force is a push or a pull; a torque is a twist. feed-forward This describes an element or pathway within a control system which passes a controlling signal from a source in the control system's external environment, often a command signal from an external operator, to a load elsewhere in its external environment. arethe S300 and AKD drives.
To use torque feed-forward, you have to rely on a CONVERTER Pipe Network block.
Use the MLCNVConnectEx function to configure the block.
The arguments must be:
- The Pipe Network block ID being configured.
- The ID of the axis to which the torque feed-forward is applied.
- The constant EC_ADDITIVE_TORQUE_VALUE.
- An ignored integer value (usually set to zero).
For more information, see:
If I measure a number (e.g., 500) as an input at the Convertor block which is connected with the PDO object (Additive Torque Value 0x60B2), how many Amps are fed in the current loop at the AKD?
Current loop feed-forward value = Rated current x IL.KBUSFF x input at converter block / 1000
Example: With an AKD where:
Rated current | 3A |
IL Instruction list - This is a low-level language and resembles assembly..KBUSFF | 1.0 |
Additive Torque (PDO object) | 500 units |
Then
IL.FF = 3 x 1.0 x 500 / 1000 IL.FF = 1.5A
There is no limitation with the cams, the number of cams, the number of cam points, etc.
The limitation is only given by the processing power of your PC.
See also see "Pipe Block Descriptions" on page 1 for more information.
Yes, I/O points represent the state of real world values.
See Use Motion Function Block for Pipe Network for this information.
The system needs to know where to place the copied blocks.
Press Ctrl-V then use the mouse to point to where you want the copied blocks to be pasted.
There are network and mechanical delays in systems that make capturing a correct pipe position Position means a point in space which is described by different coordinates. Depending on the used system and transformation it can consist of a maximum of six dimensions (coordinates).This means three Cartesian coordinates in space and coordinates for the orientation. In ACS there can be even more than six coordinates. If the same position is described in different coordinate systems the values of the coordinates are different. difficult.
To remove the delays, use a sampler block to capture the actual position of an axis.
This image shows how this works:
- This sampler block is configured to capture the actual position of axis 1.
- The conversion and axis blocks are only needed to terminate the pipe.
- MLTrigWriteDelay may still be needed to compensate for sensor A type of transducer that converts one type of energy into another for various purposes including measurement or information transfer. delay.
- If you need to calculate the master pipe value corresponding to the captured axis position, add the difference between the axis command position and the master pipe value.
If a hardware limit flag is being triggered at the program startup by a Pipe Network axis, MLAxisReAlign may need to be called immediately before motion occurs.
In this case, the distance to travel should be at least as long as the maximum distance the hardware limit flag can remain active.
Setup
The fieldbus serially links all the drives to the industrial PC.
See the figures in (➜ # 1, Different Implementations) for more information.
-
When the KAS-IDE is used to deploy an automation system on a master drive (also known as programmable drive), the fieldbus serially links all the drives to the master drive.
KAS can communicate with outside world through Ethernet, CANopen CANopen® is a communication protocol and device profile specification for embedded systems used in automation for fieldbuses working in real time., DeviceNet A communication protocol (based on Controller Area Network) used in the automation industry to interconnect control devices for data exchange. Typical applications are information exchange, safety devices, and large I/O control networks..
See (➜ # 1, Communication and Fieldbus) for more information.
Description
This issue occurs with these actions:
- Connect to the controller and download your application.
- In the Project Explorer, open the EtherCAT properties.
- Click theOnline Configuration Mode.
- In the Project Explorer, right-click the AKD_1 and select Load/Save Parameter….
- Select the Factory Defaults… command to reset New start of the microprocessor. the drive to its default parameters.
Reason
If you set the drive to its default parameters, then all the AKD parameters are restored and the unique ID (FBUS.PARAM03) used to identify the drive is lost.
Solution
You have to perform a new scan operation after setting the parameters to its default values.
-
You can also clear the Write a unique ID option in the XML Extensible Markup Language - A general-purpose markup language. It is classified as an extensible language because it allows its users to define their own tags. configuration tab.
See the click here... for more information.
If you encounter any security issues during execution of Kollmorgen Automation Suite, contact your IT department to set your proxy properly.
Firewall
You may have to define your firewall settings to allow accessing the IP addresses used by KAS (e.g., IP address of the target system or localhost IP address for the KAS Runtime Simulator: 127.0.0.1).
Port Numbers
Port numbers have to be set properly in your firewall settings to avoid any trouble during communication, such as when downloading the application to the target or plugging a probe to the Softscope.
Kollmorgen strongly recommends opening port numbers over 1024, as well as the range 502 to 520.