SAFE.ID

Description

Returns the SafeID of the device. The SafeID returned is 0, if there are no SafeID available.

SAFE.ID is accessible through telnet.

Code

--> SAFE.ID
0x31

Context

For information on validation and CRC refer to Validation.

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-00-00-000

Implemented in SMM revision v0.32

General Information

Type

Read Only

Units

N/A

Range

All

Default Value

N/A

Data Type

Integer

Stored in Non-Volatile Memory

No

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

SAFE.ID

37c2h

00h

Unsigned8

-

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

3800

1

3800 (0xed8)

SAFE.ID

Unsigned8

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

SAFE.ID

3800

Unsigned8

Read Only

-