Motion / Common - Coordinated Motion
These tables list the Coordinated Motion function blocks and function blocks:
Group Control
See Coordinated Motion - Group Control Library for more information.
|
Name |
Description |
|---|---|
|
Adds an axis to an axes group. |
|
|
Create an axis group for coordinated motion. |
|
|
Changes the state of a group to GroupDisabled. |
|
|
Changes the state of a group from GroupDisabled to GroupStandby. |
|
|
Reads a value from the specified Boolean group parameter. |
|
|
Reads a value from the specified group parameter. |
|
|
Makes the transition from the state GroupErrorStop to GroupStandby by resetting all internal group-related errors. |
|
|
Performs a controlled motion stop of all axes in the group. |
|
|
Writes a value to the specified Boolean group parameter. |
|
|
Writes a value to the specified group parameter. |
|
|
Initializes the kinematic limits for the axis group. |
|
|
Removes an individual axis from an axis group. |
|
|
Sets the kinematic transform between the Machine Coordinate System and the Axes Coordinate System. |
|
|
Removes all axes from an axes group. |
Info
See Motion / Common - Coordinated Motion - Info for more information.
|
Name |
Description |
|---|---|
|
Reads the actual acceleration of the group and the axes in the group. |
|
|
Reads the actual position of the axes in the group. |
|
|
Reads the actual velocity of the group and the axes in the group. |
|
|
Reads the command position of the axes in the group. |
|
|
Reads the command velocity of the axes in the group and the path velocity. |
|
|
Reads the Group ErrorID in state ERRORSTOP. |
|
|
Returns the status of an axes group. |
Motion
See Motion / Common - Coordinated Motion - Motion for more information.
|
Name |
Description |
|---|---|
|
Sets the default kinematic parameters for an axis. |
|
|
Converts the PLCopen |
|
|
Performs a controlled motion stop of all axes in the group. |
|
|
Sets the velocity factor that is multiplied to the commanded velocity of all axes in the group. |
|
|
Commands interpolated circular movement on an axes group to the specified absolute positions in the coordinate system as specified by the CoordSystem argument. |
|
|
Commands interpolated circular movement on an axes group to the specified relative positions in the coordinate system as specified by the CoordSystem argument. |
|
|
Commands movement of an axes group to an absolute position regardless of path. |
|
|
Commands movement of an axes group to a relative position regardless of path. |
|
|
Commands interpolated linear movement on an axes group to the specified absolute positions. |
|
|
Commands interpolated linear movement on an axes group to the specified relative positions. |
Reference
See Coordinated Motion - Reference Library for more information.
| Name | Description |
|---|---|
| MC_GrpSetPos |
Sets the axis command position for all of the axes in an axes group to the positions specified in the |