CIP Sync: Controlling the Axis and Generating Motion from the PLC

The following steps will allow the user to experiment and get familiar with triggering AOIs and the basic functionality the AOIs provide along with the basic flow of operation (See Using CIP Sync with the Kollmorgen AKD2G-SPI and Supplementary AOIs). Axis 1 (Rotary) will be used to demonstrate.