List of Figures
| Example of a help topic viewed in a large and small browser window. Note the fly-out menu on the small window. |
|
| Example of auto-completion being used to find a function |
|
| Synchronized Feeder |
|
| Spring Winding |
|
| Synchronizer |
|
| Form Fill Seal |
|
| Carton Erector |
|
| Example of Automation System |
|
| Logical Architecture Hierarchy |
|
| Architectural view of KAS components. |
|
| Hardware to Display the Human-Machine Interface |
|
| High, medium and low voltage AKD PDMMs and the PCMM. |
|
| AKD PDMM and PCMM card |
|
| Graphs comparing the performance of 800 MHz single-core, 1.2 GHz single-core, and 1.2 GHz dual-core controllers. |
|
| I/O Modules |
|
| Standard I/O Couplers and Slices |
|
| AKD |
|
| AKD2G |
|
| S300 |
|
| S700 |
|
| Kollmorgen AKM Servomotors |
|
| Cartridge Motor |
|
| Direct Drives |
|
| KAS IDEMain Window |
|
| Project Explorer with Controller type and IP address. |
|
| Configure the Device |
|
| Libraries Toolbox |
|
| Dictionary Toolbox |
|
| Dictionary Contextual Menu |
|
| Configure the Variable |
|
| Log Messages |
|
| Configuration of the Local and Controller log messages |
|
| Filtering the Messages |
|
| Filtering the Messages - Example |
|
| Find and Replace |
|
| Find and Replace from an Editor |
|
| Example of a breakpoint (Main: GT2) set in an SFC program. |
|
| Compiler Output |
|
| Watch Window |
|
| Watch Window - Accessing Arrays |
|
| Watch Window - Selecting PLC Variable |
|
| Watch Window - Creating Expression |
|
| Watch Window - Displaying Expression |
|
| Forcing a variable |
|
| AKD Toolbar |
|
| AKD Status Bar |
|
| Status Bar Labels |
|
| About Window |
|
| Log Messages |
|
| Select an Application Template |
|
| Configure the Controller Properties |
|
| Pipe Network - Open Editor |
|
| Pipe Network - Add Pipeblock |
|
| Pipe Network - Create a Link |
|
| Pipe Network - Edit a Link |
|
| Pipe Network - Delete a Link |
|
| Pipe Network - Move a Link |
|
| Pipe Network - Pipe Block Properties |
|
| Pipe Network - Mapping Axis to Drive |
|
| Pipe Network comments: editing, and deselected. |
|
| Setting Axis Units |
|
| Setting the Units - Example |
|
| Display Source Code of the Pipe Network |
|
| Motion State Machine |
|
| PLCopen Axis Context Menu |
|
| PLCopen Axis Data Dialog |
|
| PLCopen Axis Parameters |
|
| PLCopen Axis - Bus Parameters |
|
| Servo Axis - Axis Data |
|
| Servo Axis - Axis Limits |
|
| Motion State Machine |
|
| Overview of AxesGroup |
|
| Select an AKI to add. |
|
| Variable Mapping to KVB. |
|
| Open the Kollmorgen Visualization Builder Builder |
|
| AKD Configuration |
|
| AKD Setup Wizard |
|
| Add I/O Slice |
|
| Devices in the EtherCAT list and the General Properties tab of a Device's Module. |
|
| Set the Pins Number of the Block |
|
| Create a Custom Library - Select the Library Template |
|
| Use a Custom Library - Select the Library |
|
| Use a Custom Library - Display the Library |
|
| Use a Custom Library - Add a Variable |
|
| Use a Custom Library - Select the Type |
|
| Cam - New Profile |
|
| Cam - Define Profile Filename |
|
| Cam - Normalized Profile |
|
| Cam - Output Profile |
|
| Cam Profile Transformation - Step 1 |
|
| Cam Profile Transformation - Step 2 |
|
| Cam Profile Transformation - Step 3 |
|
| Cam Profile Transformation - Step 4 |
|
| Cam - Associate Profile to a Pipeblock |
|
| Set the Period of Execution |
|
| Edit the Cycle |
|
| Define the Cycle |
|
| Change Priorities by Defining the Cycle |
|
| Example of a variable not being exported and the resulting compile error. |
|
| Compiler Output |
|
| Error Location when Compiling |
|
| The Device Toolbar |
|
| Device Tooltip displays Version |
|
| Start Device with the KAS Runtime |
|
| PLC Options - Debug Compiling Mode |
|
| Setting Breakpoints |
|
| Printf Function |
|
| Customizing Output for Printf Function |
|
| Plugging a Motion Variable |
|
| Plugging a Motion Variable - Parameters |
|
| Example of Plugging a Pipe Block |
|
| Plugging a PLC Variable |
|
| Plugging a PLC Variable - Parameters |
|
| Traces Displayed with Soft Oscilloscope |
|
| Listing the Differences |
|
| Variable DictionarySee Also |
|
| Forcing a Variable |
|
| Animation in Editors |
|
| Print Project |
|
| Inserting a Reference |
|
| Defining the Reference |
|
| Autocompletion |
|
| Tooltip on Variable |
|
| Autocompletion |
|
| Tooltip on Variable |
|
| SFC Step Action Blocks |
|
| Execution Order on FBD |
|
| FBD Comments - Inserting Graphic |
|
| Add Variable in FBD Editor |
|
| Define Variable Name in FBD Editor |
|
| Define Variable Type in FBD Editor |
|
| Add a Variable in the FFLD Editor |
|
| Define a Variable Name in the FFLD Editor |
|
| Define a Variable Type in the FFLD Editor |
|
| Declare an Array for an Internal Variable |
|
| Add a Complex Structure |
|
| Rename Complex Structure |
|
| Add Variable to a Complex Structure |
|
| Create an Instance of the Structure |
|
| Edit the Name in the Variable Editor |
|
| Define Type and Scope of the Variable |
|
| Editing variables as text |
|
| Errors caused by editing variables. |
|
| Parameters and Private Variables |
|
| Create an Instance of UDFB in a Program |
|
| Global Defines |
|
| Edit the Global Definitions |
|
| Wizard to Create PLC Variable - Parameters |
|
| Wizard to Create PLC Variable - Mapped Channels |
|
| Wizard to Create PLC Variable - Variables in the Dictionary |
|
| EtherCAT Devices Summary Form |
|
| EtherCAT Network - Physical View |
|
| EtherCAT Network - Logical View. K-Bus on left, E-Bus on right |
|
| EtherCAT Master Settings |
|
| ENI File tab |
|
| The ESI Files tab |
|
| Do not overwrite these files. |
|
| Opening — Upon opening a KAS project, the project's ESI files are compared to the internal library. If there are conflicts, you are prompted to resolve them. |
|
| Adding/Deleting — Adding or deleting an ESI file from the KAS IDE affects KAS's internal library of ESI files. |
|
| Saving — When a KAS project is saved, a copy of the ESI file(s) is included in the project file. |
|
| The PDO Selection/Mapping tab including FSoE objects in yellow. |
|
| The PDO Editor tab |
|
| Examples of live checking for valid entries. |
|
| Example of a device with oversampling. |
|
| Example of a Parallel Sequence in SFC |
|
| Regulation with Remote Drive |
|
| Multi-Axis Driven by a Virtual Master |
|
| Hardware Organization of Motion Functions |
|
| Third-order motion profile |
|
| Mechanical System |
|
| Pipe Network Structure |
|
| Typical Pipe Structure |
|
| Axis Pipe Block Positions |
|
| Motion State Machine |
|
| List of Pipe Blocks |
|
| TMP Parameters: INITIAL_POSITION and TRAVEL_SPEED |
|
| TMP Parameters: ACCELERATION and DECELERATION |
|
| TMP Parameters: MODE "No Modulo" |
|
| TMP Parameters: MODE Modulo and MODULO_POSITION |
|
| PMP Generator forward & backward motion profile |
|
| PMP Parameters: FIRST_TRAVEL_SPEED, LAST_TRAVEL_SPEED and ACCELERATION |
|
| PMP Parameters: INITIAL_POSITION, "No Modulo" and MODULO_POSITION |
|
| PMP Motion Profiles for a Relative Move |
|
| PMP Motion Profiles for a Forward-Backward Motion |
|
| Sampler |
|
| Sampler Period |
|
| Sampler Mode Position |
|
| Sampler Mode Speed |
|
| Sampler Pipe Block Used to Track an External Master |
|
| Synchronizer Pipe Block to Start, Stop and Re-synchronize a Slave Axis |
|
| Derivator - "No Modulo" Mode |
|
| Derivator - Modulo Mode |
|
| Integrator - "No Modulo" Mode |
|
| Integrator - Modulo Mode |
|
| Trigger Extrapolates Output Value Based on Fast Input Timestamp |
|
| Cam Parameters |
|
| Cam Blocks Control Operation of a Three Axis Filling Mechanism |
|
| Comparator Used to Control a Valve on a Filler Mechanism |
|
| Convertor - Position Mode "No Modulo" |
|
| Convertor - Position Mode (Modulo) |
|
| Convertor - Speed Mode |
|
| Define Value with Expressions |
|
| Mode Modulo |
|
| Mode "No Modulo" |
|
| Axis Parameters: INITIAL_POSITION and TRAVEL_SPEED |
|
| Axis Parameters: ACCELERATION and DECELERATION |
|
| Axis Parameters: MODE "No Modulo" |
|
| Axis Parameters: MODE Modulo and MODULO_POSITION |
|
| Small Jerk Acceleration |
|
| Large Jerk Acceleration |
|
| Trapezoidal Acceleration |
|
| Graphic of how PLCopen axis position data is calculated. |
|
| How Actual Position is calculated. |
|
| Motion State Machine (PLCopen) |
|
| Versatile Network Architecture |
|
| Process Data is Inserted in Telegrams |
|
| Flexible Topology: Line, Tree or Star |
|
| Synchronicity and Simultaneousness |
|
| Safety over EtherCAT Software Architecture |
|
| Fieldbus Gateway |
|
| Several Device Profiles and Protocols can coexist |
|
| Master-Implementation with one Process Image |
|
| Structure of EtherCAT Master Implementation |
|
| EtherCAT Network Architecture1Image courtesy of EtherCAT.org, http://www.ethercat.org/pdf/english/etg2200_v2i0i1_slaveimplementationguide.pdf |
|
| Slave Hardware: FPGA with Host CPU |
|
| Slave Hardware: FPGA with direct I/O |
|
| EtherCAT State Machine |
|
| CANopen Status Machine |
|
| AKD Configuration According to EtherCAT State |
|
| Priority Between Motion and PLC |
|
| Application Overrunning the Basic Cycle |
|
| Firewall alert dialog. |
|
| KAS Runtime Log Window |
|
| Axes Tab |
|
| Set Axis in Error Mode |
|
| Deselect an Axis |
|
| KAS Simulator Main Window |
|
| Options for KAS Simulator |
|
| The Webserver Tabs as seen on an AKD PDMM webserver. |
|
| Example of log files displayed from a AKD PDMM or PCMM webserver. |
|
| Example of a log file's content, displayed in a browser. |
|
| Example of a AKD PDMM or PCMM with a manually defined IP address |
|
| File System tab on an AKD PDMM or PCMM web server, and when using Simulator. |
|
| Pipe Network Structure |
|
| Pipe Network - Create a Link |
|
| Pipe Block - Relation Type for Output-Input |
|
| A cam profile |
|
| Cam Profile Editor Main Window |
|
| Cam Table |
|
| Modifying an Element Type |
|
| Cam Table Contextual Menu |
|
| Add New Point |
|
| Cam Table Contextual Menu |
|
| Cam Profile Graph |
|
| Cam Profile Graph - Slope Line |
|
| Cam Profile Graph - Contextual Menu |
|
| Curve Selection Table |
|
| Standard Color Selection |
|
| Curves Graph |
|
| Example of using the Oscilloscope |
|
| Accessing the Scope |
|
| Oscilloscope Control Panel |
|
| Scope Control Panel - Channels |
|
| Scope Control Panel - Time-base |
|
| Scope Control Panel - Time Position |
|
| Cycle Time Calculation |
|
| Motion, PLC and Real Time Margin Time Calculations |
|
| Multiple Core Controller, PLC and Real Time Margin Time Calculations. |
|
| Example of the traces generated in the Oscilloscope. |
|
| Using the Variable Selector to choose a variable to be mapped in the Oscilloscope |
|
| Plugging a Probe from the Dictionary |
|
| Associating a PipeNetwork (left) and PLCopen (right) variable to a Channel |
|
| Plugging a Probe from the Pipe Network |
|
| Control Panel Control Library |
|
| Control Panel Control Properties |
|
| Control Panel - Selection of Controls |
|
| Map variables to a Control Panel control |
|
| Map Variables to a Control Panel Control in the Graphical Editor |
|
| Control Panel |
|
| Display of KAS Simulator |
|
| Examples of CS types on a machine and part. |
|
| n-Degree Transition |
|
| 180-Degree Transition: New move is in the opposite direction as old move. The sudden change in the direction of motion may result in large jerks to the axes |
|
| 0-Degree Transition: New move continues in same direction as old move — continuous behavior |
|
| 0-Distance Transition: Motion passes the first move's endpoint . There is no transition arc. A sudden change in the direction of motion may result in large jerks to the axes. |
|
| n-Degree Transition |
|
| Tangent Transition: Line is tangent to the arc |
|
| Intersection Transition: The line intersects the arc a "corner distance" away from the beginning of the new move. |
|
| 0-Distance Transition: Special behavior for 0-distance transitions. |
|
| Examples of Arc-to-Arc Transitions |
|
| Oscilloscope Representation of linear coordinated move with a MC_GrpHalt command called twice |
|
| Oscilloscope Representation of linear coordinated move with a MC_GrpStop |
|
| Online Change - Process Diagram |
|
| Online Change - States and Transitions |
|
| PLC Options - Online Change Enable |
|
| Online Change - Updating Controller Version |
|
| Online Change - Dictionary |
|
| One-click Recovery - Process Diagram |
|
| Pulse Limitations with Falling Edge |
|
| Pulse Limitations with Rising Edge |
|
| Registration |
|
| Example of using a Pipe Network Trigger block for position capture. |
|
| Configuration of the Trigger block |
|
| PLC Timestamp Related to Fast Input Event |
|
| Example of setting byte sizes in a third-party Network Configurator. |
|
| Example of setting byte sizes in the KAS IDE Fieldbus Editor |
|
| Example of configuring sub-modules. |
|
| Software Structure Overview |
|
| Main Module Description |
|
| Axis Module Description |
|
| State Machine |
|
| PN Template with FFLD - Main |
|
| PN Template with ST - Main |
|
| PN Template - Main |
|
| PN Template - MachineLogic |
|
| PN Template - Motion |
|
| PN Template - Control Panel |
|
| PN Template with ST - Main |
|
| PN Template - Motion |
|
| PN Template - Control Panel |
|
| PN Template with FFLD - Main |
|
| PN Template - Motion |
|
| PN Template - Control Panel |
|
| PLCopen Template with FFLD - Main |
|
| PLCopen Template with ST - Main |
|
| PLCopen - Template Main |
|
| PLCopen Template - Step 5 of the Main |
|
| PLCopen Template - Motion |
|
| PLCopen Template - Control Panel |
|
| PLCopen Template - Fault Report Panel |
|
| PLCopen Template with ST - Main |
|
| PLCopen Template - Motion |
|
| PLCopen Template - Control Panel |
|
| PLCopen Template - Fault Report Panel |
|
| PLCopen Template with FFLD - Main |
|
| PLCopen Template - Motion |
|
| PLCopen Template - Control Panel |
|
| PLCopen Template - Fault Report Panel |
|
| SFC step action blocks |
|
| SFC Time Diagram - Timer vs Step Activation |
|
| List of Pipe Blocks |
|
| MLPipeAct |
|
| MLPipeAddBlock |
|
| MLPipeDeact |
|
| MLBlkReadModPos |
|
| MLBlkReadModPos |
|
| MLAddInit |
|
| MLAddReadOff1 |
|
| MLAddReadOff2 |
|
| MLAddReadRatio1 |
|
| MLAddReadRatio2 |
|
| MLAddWriteInput |
|
| MLAddWriteOff1 |
|
| MLAddWriteOff2 |
|
| MLAddWriteRat1 |
|
| MLAddWriteRat2\ |
|
| Initial speed is smaller than the new speed |
|
| Initial speed is bigger than the new speed |
|
| The speed update is taken into account only if the second MLAxisAbs is triggered during acceleration or constant velocity |
|
| ML_AxisDriveNumber |
|
| Axis Functions Usage |
|
| MLPrfReadIOffset |
|
| MLPrfReadIScale |
|
| MLPrfReadOOffset |
|
| MLPrfReadOScale |
|
| MLPrfWriteIOffset |
|
| MLPrfWriteIScale |
|
| MLPrfWriteOOffset |
|
| MLPrfWriteOScale |
|
| MLCompCheck |
|
| MLCompWriteRef |
|
| Comparator Functions Usage |
|
| MLCNVConnect |
|
| MLDerInit |
|
| MLDerReadInModPos |
|
| MLDerWriteInModPos |
|
| Gear Functions Usage |
|
| MLIntInit |
|
| Master Functions Usage |
|
| Initial speed is smaller than the new speed |
|
| Initial speed is bigger than the new speed |
|
| The speed update is taken into account only if the second MLAxisAbs is triggered during acceleration or constant velocity |
|
| TMP Initialization |
|
| Phaser Functions Usage |
|
| PMP Generator Forward & Backward Motion Profile |
|
| MLSmpConECAT function |
|
| MLSmpConPLCAxis function |
|
| MLSmpConPNAxis function |
|
| MLTrigIsTrigged |
|
| MLTrigReadPos |
|
| MLTrigReadTime |
|
| Trigger Functions Usage |
|
| MC_ClearFaults |
|
| MC_CreatePLCAxis |
|
| MC_EStop |
|
| MC_InitAxis |
|
| MC_InitAxisFeedback |
|
| MC_Power |
|
| MC_ErrorDescription Function Block |
|
| MC_ResetError |
|
| MC_Stop |
|
| MC_TouchProbe |
|
| MC_ReadActPos |
|
| MC_ReadActVel |
|
| MC_ReadAxisErr |
|
| MC_ReadBoolPar |
|
| MC_ReadParam |
|
| MC_ReadStatus |
|
| The MC_WriteParam function block |
|
| MC_Halt |
|
| MC_MoveAbsolute |
|
| MC_MoveAdditive |
|
| MC_MoveRelative |
|
| MC_MoveSuperimp |
|
| MC_MoveVelocity |
|
| MC_MoveContVel |
|
| MC_SetOverride |
|
| MC_CamIn |
|
| MC_CamIn examples |
|
| MC_CamOut |
|
| MC_CamStartPos |
|
| MC_CamStartPos |
|
| MC_GearIn |
|
| MC_GearInPos |
|
| MC_GearOut |
|
| MC_Phasing |
|
| MC_SyncSlaves |
|
| MC_Reference |
|
| MC_SetPos |
|
| Motion State Machine |
|
| MC_AddAxisToGrp |
|
| MC_CreateAxesGrp |
|
| MC_GrpDisable |
|
| MC_GrpEnable |
|
| MC_GrpReadBoolPar |
|
| MC_GrpReadParam |
|
| MC_GrpReset |
|
| MC_GrpWriteBoolPar |
|
| MC_GrpWriteParam |
|
| MC_InitAxesGrp |
|
| MC_RemAxisFromGrp |
|
| MC_SetKinTra |
|
| MC_UngroupAllAxes |
|
| MC_GrpReadActAcc |
|
| MC_GrpReadActPos |
|
| MC_GrpReadActVel |
|
| MC_GrpReadCmdPos |
|
| MC_GrpReadCmdVel |
|
| MC_GrpReadError |
|
| MC_GrpReadStatus |
|
| MC_AxisSetDefaults |
|
| MC_GrpSetOverride |
|
| MC_MoveCircAbs |
|
| MC_MoveCircRel |
|
| MC_MoveDirAbs |
|
| MC_MoveDirRel |
|
| MC_MoveLinAbs |
|
| MC_MoveLinRel |
|
| MC_GrpSetPos |
|
| DriveParamRead |
|
| DriveParamStrRead |
|
| DriveParamWrite |
|
| ECATReadSdo |
|
| ECATReadSdo State Diagram |
|
| ECATWriteSdo |
|
| ECATWriteSdo State Diagram |
|
| ECATCommErrors function block |
|
| ECATDeviceStatus function block |
|
| ECATMasterStatus function block |
|
| ECATWCStatus function |
|
| GetCtrlPerf |
|
| The FileCopy Function Block |
|
| The FileCopy Function Block |
|
| The FileDelete Function Block |
|
| The FileCopy Function Block |
|
| The FileExists Function Block |
|
| The FileOpenA function block |
|
| The FileOpenR function block |
|
| The FileOpenW function block |
|
| The FileReadBinData Function Block |
|
| The FileReadLine Function Block |
|
| The FileRename Function Block |
|
| The FileCopy Function Block |
|
| The FileSize Function Block |
|
| The FileWriteLine Function Block |
|
| The FileWriteLine Function Block |
|
| The TcpAccept function block |
|
| The TcpBinReceive function block |
|
| The TcpBinSendf function block |
|
| The TcpClose function block |
|
| The TcpConnect function block |
|
| The TcpIsConnected function block |
|
| The TcpIsValid function block |
|
| The TcpListen function block |
|
| The TcpSend function block |
|
| CBS First Order Digital Filter |
|
| Pulse Width Duty Cycle |
|
| Scale Input |
|
| Scale Output |
|
| FB_ElapseTime |
|
| MFB_ElapseTime – Time Diagram |
|
| PipeNetwork_FFLD |
|
| ProfilesCode_FFLD |
|
| The TemperaturePID user-defined function block |
|
| Mode to find the zero angle reference of the motor. |
|
| MLFB HomeFindHomeFastInput |
|
| MLFB HomeFindHomeFastInputModulo |
|
| MLFB HomeFindLimitFastInput |
|
| MLFB HomeFindLimitFastInputModulo |
|
| Kollmorgen UDFB Jog for PipeNetwork |
|
| MCFB_AKDFault |
|
| MCFB_AKDFaultLookup |
|
| MCFB StepAbsolute |
|
| MCFB StepAbsSwitch |
|
| MCFB StepBlock |
|
| MCFB StepLimitSwitch |
|
| MCFB StepRefPulse |
|
| MCFB StepAbsSwitchFastInput |
|
| MCFB StepLimitSwitchFastInput |
|
| Jog for PLCopen |
|
| MCFB_GearedWebTension Function Block I/O |
|
| AKDFltRpt |
|
| S700FltRpt |
|
| Form Fill and Seal Machine Overview |
|
| Filling Screw Base Profile |
|
| Sealing Jaw Base Profile |
|
| Flying Shear Base Profile |
|
| Form Fill and Seal Machine Overview |
|
| Filling Screw Base Profile |
|
| Sealing Jaw Base Profile |
|
| Flying Shear Base Profile |
|
| Unwind Base Profile |
|
| Cutting Knife Base Profile |
|
| Unwind Base Profile |
|
| Cutting Knife Base Profile |
|
| Knife CAM profile |
|
| Rotary Knife Pipenetwork |
|
| Knife Cam profile |
|
| Feeder CAM Profile base shape |
|
| Mapping of standard components |
|
| Standard Components in Project tee |
|
| EtherCAT structure in the dictionary |
|
| EtherCAT function blocks in the library. |
|
| Standard Components in the Project View. |
|
| Standard Components in the EtherCAT view. |
|
| Start view of the EtherCAT Configurator |
|
| General view with the EtherCAT nodes |
|
| PDO Assignment |
|
| Task view |
|
| Variable view |
|
| Device EtherCAT view |
|
| KAS IDE EtherCAT ENI File view |
|
| EtherCAT address setting for AKD drives |
|
| XML image showing Output Index number for Axis1 and Axis2 |
|
| XML image showing Input Index number for Axis1 and Axis2 |
|
| Example of data index offset and size for non-standard I/O item |
|
| Direct EtherCAT function blocks in KAS IDE library |
|
| Writing to a non-standard I/O device |
|
| Complete XML file mapping – part 1 |
|
| Complete XML file mapping – part 2 |
|
| SFC Step - Timeout Alarm |
|
| The file cclog.txt is not writeable. |
|
| The file main.c is not writeable. |
|
| ETHERCAT Coupler Diagnostic LEDs |
|
| Connecting all the Hardware components |
|
| The TcpReceive function block |
|